Team,
We are using HDC2021 and we have few observations and we would like to clarify .
Settings
Sensor Supply Voltage : 3.3 V
Frequency 100KHz
With the above are the settings we face 2 issues .
#1. when we read all register settings from the sensor we could read the settings which is written by us and temperature , humidity registers are 0. I have mentioned the data which is read from the sensor
Register values - 00,00,00,00,00,00,00,60,00,00,45,69,00,ff,54,00#
#2. Sometimes the adc values of temperature and Humidity from sensor is 0 and FFFF .Please help with this as we are facing these kind of issues frequently