Hi Team:
I have a design requirement for smart lamp on customer side, can you help to verify if IWR6843 meet the design target, thanks!
The basic requirement is as below:
1. Use sensor to grasp the movement around the lamp. Radar sensors are or Ultrasonic sensor or PIR sensors can be proposed, which one is better? pls advise
2. The motion sensor can be set and changed by setting the detection range in at least 3 stages (*).
* * The detection range of the motion sensor is centered on 2, 3 meters directly below the lamp, for example ≦1m / ≦2m / ≦3m