I checked the coil design tool according to the information you provided, but which items are required for LDC0851?
◎Racetrack Inductor Design
Sample Rate Calculator
×Indcutance and Frequency from Output Code
◎Skin Depth Calculation
×LDC16X...
×◎LDC1XX...
◎Remote Coil Maximum Distance Claculator
◎LDC0851 Calculator Tool
×LDC1101...
Spring Sensor Calculator Tool
◎: Necessary item, ? ◎: Required, ?: Unknown, X: Not required.
We found that the target size depends on the sensor coil, but the small target 50mm x 50mm is the maximum realistic target size as described in Inductive Sensing: Target size Matters.
Is 50 mm x 50 mm the maximum realistic target size?
The target size that we want is more than 1000mm x 1000mm.
Is it possible to design a sensor that can handle that?
I haven't read all the manuals carefully, but I would like to confirm whether or not the LDC0851 can be installed.
I have not read all the manuals thoroughly, but I would like to confirm whether the LDC0851 can be installed or not, so please answer me as concretely as possible.