I am using 6 layers, 1 oz, 2 mm PCB and would like to design a 7mm diameter sensor.
I noticed that web tools are capable to export PCB files to a maximum of 4 layers designs.
From performance and resolution aspects - is it better to design 6 layers sensor or 4 layers sensor assuming diameter is kept
constant?
if I would like to avoid the external influence of metal that are not the target :
- is it better to spread the 4 layers sensor design across 6 layers, leaving 2 unused layers in the middle of the PCB or
is it better to use 4 layers sensor located close to the target side, leaving 2 empty layers?
thanks