Other Parts Discussed in Thread: TIDEP-0091
Procedure: Level_sense_demo in TIDEP-0091
Step: Change the frameCfg-> numFrames in the program from 1 to 0, and add demo_config1D_HWA(dataPathObj);demo_dataPathTrigger1D(dataPathObj); at the end of each measurement, enables radar software to trigger measurements continuously.
Distance Value Target: Select the distance chirp_data.distance[0] from the point of maximum signal strength obtained in demo_findTopTanges
Range: Chirp Budget Calc_09_25_18 of sprcah9.
Question: the customer would like to know why the error is so large
1. Range With DEMO_CONFIG 30: the actual test will basically not measure the distance value at more than 20 meters.
2.Range With DEMO_CONFIG 75: the actual measurement can measure 70 meters, but the error is about 1 meter at 50 meters, about 1.5 meters at 60 meters, and over 2 meters at 70 meters.
Best Regards,
Cherry Zhou