Other Parts Discussed in Thread: PGA460
Hello Sir/Ms.
Our customer is asking whether PGA460-Q1 meets the ISO26262 specification? I can't see such a description in the specification. Customers say that the Elmos .09 they are using complies with ISO26262. He wanted to use the PGA460 as a distance detection in a moving car. Does our PGA460-Q1 comply with the ISO26262 specification? If not, is there a recommendation?
Best Regards,
Kami Huang