Other Parts Discussed in Thread: TMP117, TMP1075
HI, staff
Let me ask you a question in Absolute Maximum Ratings of TMP102-Q1 (SBOS702E).
The Min value of the Supply voltage is -0.3V.
However, the Min values for SCL, SDA, ADD0, and ALERT are -0.5V.
Is it okay to understand that applying a voltage -0.5V lower than the min value of the power supply -0.3V does not affect the signal terminals?
The voltage min value for the signal line of the same function device such as TMP117, TMP1075 is -0.3V, which is the same as the power supply terminal.
best regards
cafain