Now I want to get the temperature of the AWR1642, and I get the data by calling the following function periodically:
rlRfTempData_t Temp_Data;
rlRfGetTemperatureReport(RL_DEVICE_MAP_INTERNAL_BSS, &Temp_Data);
When I first power on, I can get the temperature of the AWR1642, but the data change needs too much time, and the data jump range is very large.
I got the data in 1s, 3.3s, 10s cycles, the phenomenon is the same.
Q: Is there any way to get the real time temperature?