HI everyone,
I am tying to install the mmwave-sdk 02.01.00.04 on an up-to-date Ubuntu 18.04 64bit. The installer asks me what I want to install, I select everything and start the installation. The progress bar goes to 100% fairly quick and is then stuck at 100%. The "I am doing something"-indicator is rotating, but nothing happens any more, even after an hour. There is no CPU/disk/network traffic. Below is a screenshot.
Any ideas how to fix that?