Part Number: AMC6821EVM-PDK
From the user guide we understood that , this EVM software needs windows 2000/XP.
We have prepared an Windows XP with SP3 installed PC but the EVM is still appearing as "unknown" in Device manager.
We request your help in resolving this soon so that we can work with actual device.
With this experiment we have few open questions as below.
Which Windows XP edition is supported with this EVM ? home/professional edition of windows xp ?
Which service pack is required ? Windows XP SP1/SP2/SP3 ?
Do we need any additional drivers other than the ones provided on CD to make this EVM correctly with the software ?
If correctly installed , what is the name of the device which appears in device manager for this EVM ?