This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT8320: 3D TOF sensor for visible light spectrum

Part Number: OPT8320
Other Parts Discussed in Thread: OPT8241,

Question 1:

 Data sheet specifies that OPT8241/OPT8320 has  Integrated Optical Band-Pass Filter (830 nm to 867 nm) .This restricts us from using this sensor as we are planning to use this product in visible range

Also is there a way that this filter can be bypassed or customized for our use as this is a huge bottleneck in allowing us to use the product.

Question 2:

Are these parts available for purchase?