Other Parts Discussed in Thread: IWR6843AOPEVM,
Hi,
We have been working on using IWR6843AOPEVM for altimetry on an industrial drone.
We want to interface IWR6843AOPEVM with an Linux/ARM64 (Jetson Nano)
Previously, one TI expert mentioned it is easy to use the serial peripherals (USB,SPI, UART, I2C) to connect to a Linux/ARM64 host
Here are the issues:
1- SDK does not seem to support ARM64 (although it may be available for Ubonto). So USB communication is not an option with Linux/ARM64
2- I2C port which is available on AWR6843AOPEVM (through a 4-pin connector) does not seem to provide RADAR data (e.g., range, point cloud, etc). It is for PMIC, temperature etc.
Question:
Is there anyway to interface AWR6843AOPEVM with Jetson Nano through USB or serial peripherals?
Thanks,
POUYA