Hi Experts
The customer want to config a chrip with three TXs at different start frequency. This there a method to achieve this ?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Experts
The customer want to config a chrip with three TXs at different start frequency. This there a method to achieve this ?

Hi,
Yes, this is possible,
Depending on the different start frequencies, this can be achieved in two ways.
If there is a larger difference between the start frequencies, different profiles can be used for each of the 3 chirps. There are 4 profile configurations available.
If there is a small difference in the start frequency, different start frequencies can be defined in the chirp configuration (START_FREQ_VAR)
The ranges of the chirp configuration START_FREQ_VAR is provided in the Radar Interface Control Document available in the Device Firmware Package
Thank you
Cesar
Hi, Cesar
Thanks for your response, that I wants consult if a method that config one chrip with three TXs work at same time but they have different start frequency, such as in 1 chrip the Tx0's start frequency is 79.0GHz, the Tx1's start frequency is 79.1GHz, the Tx2's start frequency is 79.2GHz.
As your advice that will use 3 chrips to achieve these three different star frequencies.
Thanks