Other Parts Discussed in Thread: IWR1443,
Hello,
We are in the process of evaluating the IWR1443 76-81GHz FMCW Radar senor for use in both liquid and solids level sensing and have performed tests with both high and low dielectric from water to oil, cereal, sand, and others. Compared the results of IWR1443BOOST with an existing 80GHz FMCW Radar level sensor already on the market and provided the test result comparison file for your reference. The IWR1443 (without lens) performed very well using the High Accuracy precompiled firmware and High Accuracy Visualizer utility to measure wave forms and peaks. What we found in comparing the radar sensor already on the market was the linearity of the measurements were considerably more consistent than the IWR1443BOOST. We are looking for your recommendations regarding how to improve the accuracy similar to the application note for the 100meter tank with mm accuracy and some additional questions provided below. Please see attached files with comparison tests and general test setup. Any help you can provide would be appreciated.
- Do you have any lens/antenna recommendations for the IWR1443BOOST demo board which would help improve accuracy and effectiveness of the signal? Please provide manufacture and part number? Does TI offer any assistance for the development of lens or antenna?
- In the software are there any additional measures that can be adopted or currently exist that would improve the accuracy? Sweep of frequencies and power output variances which may help detect and provide for false signal suppression, and optimization for various dielectric constants within the 77-81GHz frequency range?
- What measures can be taken to insure optimum signal to noise ratio?
- What settings in the configuration would help improve the accuracy beyond the results found in tests with 2000ml beaker and 135gallon plastic tank? Any recommendations would be greatly appreciated.
Please let me know if you have any questions or need additional information.
Link to test file comparison
https://drive.google.com/drive/folders/14eHC8ShLAXhw_hEPJSJZViIc6fvBqK9V?usp=sharing
Thank you very much for your time,
Glen Kalchbrenner