This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: IWR1843BOOST

Part Number: IWR1843BOOST


Hi,

pressed the wrong button, meant to REPLY!  One last question on this then I will close the thread - promise!

I suspect the answer may be either that this is too deep to discuss here, or that on the lines of that's what the SDK means by "only s/w trigger supported"...

trying to use h/w trigger, things do happen (as seen in output) but, even though it seems to say everything has completed just as it does for s/w trigger, trying to do another run leads to the response:

 Status: Failed, Error Type: API IS ISSUED WHEN FRAMES ARE ONGOING

Is there anything I can send API wise to recover from this, other that a complete hard restart of everything (STOP FRAME doesn't seem to do it)?  Or is it that I need to send multiple triggers (per frame?) rather than just once to start things off?

many thanks

Alan