Other Parts Discussed in Thread: IWR6843ISK, DCA1000EVM,
Hi allI am using the IWR6843ISK, the MMWAVEICBOOST and the DCA1000EVM.
I believe I have connected all cables right (one 5V/2.5A on the DCA1000EVM, one 5V/2.5A on the ICBOOST, one micro USB on XDS110 on ICBOOST, one micro-USB on FTDI on DCA1000EVM and the ethernet cable on DCA1000EVM).
I have also set all the DIP switches as per MMWAVEICBOOST documentation.
With these settings everything was working fine. By everything I mean I could capture raw data using mmWave Studio.
Now I removed R346 on the ICBOOST and put a 0 Ohm resistor across R348. I did this because I want to trigger/start the data collection using hardware i.e a rising edge on pin 9 of J15 on ICBOOST.
Now the problem is that RS232 Connection is failing on mmwave studio with error: RadarAPI]: Error: Connection failed: Calling_ConnectTarget returned 3.May someone please assist me debug my setup.