Other Parts Discussed in Thread: AWR1843
Hi there,
I'm working on AWR1843BOOST Evaluation Module and I'm studying with resource explorer codes (/software/mmWave Sensors/Automotive Toolbox (3.4.0)/Labs/Medium Range Radar) Accordingly, I would be very grateful if you could answer my questions below.
- If I understand correctly, CCS Project - DSS codes for AWR1843 sensor, CCS Project - MSS codes for TM4C1294NCPDTT3 microcontroller. Am I right?
- I want to transfer distance and speed data by communicating with the TM4C1294NCPDTT3 microcontroller on the AWR1843BOOST development board and another microcontroller from outside with minimal changes in the code. I don't need to connect it to a computer, to simulate it.
- If I am not going to communicate with the computer and simulate it, which parts of the code should I remove?
- If I am going to communicate with another microcontroller, which communication protocol should I use?
- Do you have an example used in the TM4C1294NCPDTT3 microcontroller for the communication protocol you suggest?
- Can you summarize which code file in CCS Project - DSS or CCS Project - MSS was written for which functions?