Hi.
The I2C clock frequency is defined below in the AC characteristics of the TMP117 specifications.
Frequency: MAX400kHz
tLOW: Min 1300ns
tHIGH: Min 600ns
When CLK = 400kHz and Duty = 50%, both tLOW and tHIGH are 1250ns, which does not meet the above tLOW specifications.
In the specifications, Duty is about 1: 2, but in general-purpose microcomputers, Duty = 50% CLK is common and there is a contradiction in the specifications.
It works fine in terms of ability, but what should I think about this spec?