Other Parts Discussed in Thread: DCA1000EVM
Dear Expert
Good day!
Our customer need to confirm the details below :
I need some information to capture raw data, to my fpga board
mmwave_dpf package
mmwave_studio_package
1)mmwavelink_example : Is used to trigger the awr1243-boost .
Is that i can triggers the radar by using any launch-pad of TI ,for example : I have a launch pad of TM4C1294XL
can i overwrite the source-code of "mmwavelink_example" to TM4C1294XL-launchpad and can trigger the rader instead of DCA1000EVM..?
2)mmwave_studio_package:It has DCA1000EVM_CONTROL.exe to catch the raw data from radar after the data trigger from radar using "mmwavlelink_example".
Is that i can use and fpga board which has LVDS and CSI port to catch the RAW_data and do post processing ,is that possible...?
BR,
Leon.liu