I'm considering a prototype using OPT3101.
The MCU that controls the OPT3101 will be selected from other companies. What is the program size (RAM, ROM) required to control the OPT3101?
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm considering a prototype using OPT3101.
The MCU that controls the OPT3101 will be selected from other companies. What is the program size (RAM, ROM) required to control the OPT3101?
Best Regards,
Hi,
Please refer to the OPT3101 SDK online. This is the MCU code we recommend for performing OPT3101 calibration and it also has code for running as well.
Best,
Alex
Thank you for your quick response.
What is the program size of the OPT3101 SDK?
Which file in the OPT3101 SDK can I use to check the program size?
Regards,
Hi,
I am not sure the exact size and this would also vary by MCU used. You would need to compile the code for the MCU to see the size.
Best,
Alex