I'm currently looking at an application where I'm interested in the values that are primarily filtered out currently as noise.
I'm able to track the over all noise level using the mmWave demo and it's responding as the mathematical theory predicts it should in response to the specific characteristics i'm looking at so that's a good start. However, i'm wondering if it's possible to get more detail. so my question is multi part.
1. I want to evaluate a cloud of moving particles at a fairly close range. In any given second there may be thousands or 10's of thousands of particles in the field of view. I can see the impact these particles have as a surge in the noise level but how much data is actually being received for the noise and how is the sum noise level calculated?
2. Do the "noise" signals have recorded direction and strength?
3. Does the DCA1000 board allow for the recording and parsing of individual returned signals, whether they are seen as noise or object?
4. Is there a practical limit to the maximum number of signals that can be processed per chirp? I'm not sure how many signals I need to process per chirp but the more the better.
5. Can the radar be set up to just observe particles at Z distance away from the transceiver and X-X distance to the right or left? I.E. flat horizontal plane extending out from the transceiver and to ignore anything that is above or below the normal plane relative extending perpendicular from the face plane of the transceiver? I just want to get a horizontal slice through my particle field.
I want to be able to just look at the noise and completely ignore any non-moving, stationary objects.