I asked a similar question 1 month ago about 6843ODS not responding to ceiling-mount cfg using 3D people counting demo. Here is the link
The problem with ODS is not solved using other visualizer GUI. . As posted below, we are using the default cfg according to 3D_people_counting_detection_layer_tuning_guide.pdf. We think the problem is with the cfg file, because everytime we successfly send a working cfg file and the aop board start to run, the top right USQ_LED light will be on and flicker. But after sending ceiling mount cfg, the light is off and no response from the visualizer. Can you tell us what is wrong with the ceiling mount cfg from guide document or do you have any proved working ones?
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
lowPower 0 0
profileCfg 0 61.2 60.00 17.00 50.00 394758 0 55.27 1 64 2000.00 2 1 36
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 224 0 120.00 1 0
dynamicRACfarCfg -1 10 1 1 1 8 8 6 4 4.00 6.00 0.50 1 1
staticRACfarCfg -1 4 4 2 2 8 16 4 6 6.00 13.00 0.50 0 0
dynamicRangeAngleCfg -1 7.00 0.0010 2 0
dynamic2DAngleCfg -1 5 1.000 1 1 15 2
staticRangeAngleCfg -1 0 1 1
antGeometry0 -1 -1 0 0 -3 -3 -2 -2 -1 -1 0 0
antGeometry1 -1 0 -1 0 -3 -2 -3 -2 -3 -2 -3 -2
antPhaseRot -1 1 -1 1 -1 1 -1 1 -1 1 -1 1
fovCfg -1 60.0 60.0
compRangeBiasAndRxChanPhase 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
staticBoundaryBox -3 3 -3 3 -0.5 3
boundaryBox -4 4 -4 4 -0.5 3
sensorPosition 2.9 0 90
gatingParam 3 2 2 3 4
stateParam 3 3 6 20 3 1000
allocationParam 20 20 0.05 20 1.5 20
maxAcceleration 1 0.1 1
trackingCfg 1 4 800 20 37 33 120
sensorStart