Other Parts Discussed in Thread: DRV5053, DRV5056, DRV5055
I have been using the DRV5053 hall effect sensors to measure the change in magnetic field of a permanent magnet. I am using several sensors at once and the problem I am having is that the sensors are not very consistent with each other. I am seeing up to a 60mV difference between sensors when not in a magnetic field. I get similar results when I subject all the sensors to the same magnetic field. I am looking for a change of around 100mV (a little over 1mT since 90mV/mT for this sensor) as a trigger so 60mV is very significant. I should add that I am filtering the power and signal as recommended by the data sheet.
I have ordered some DRV5056 sensors for more resolution since I only need to measure in one direction. I have seen on your forums that they have a higher accuracy. The data sheet shows a lower noise level than the DRV5053. I am also looking into adding in a low pass filter to shorten the range to reduce the noise as recommended by the data sheet. In addition to these improvements, is there any kind of calibration sequence that is recommended for these type of sensors? Or any other way to improve accuracy over a small range? Are there other sensors I should be using instead?
Please let me know if I am on the right track.