Other Parts Discussed in Thread: IWR6843AOP
hello,
I am looking to have 1D/2D FFT data out of my sensor as they are of better use for my study.
To get 2D-FFT data (Doppler-Range heatmap) I started by increasing the baudrate of the dataPort to 3125000, and set guiMonitor to -1 0 0 0 0 1 0
Doing this, I was able to increase the frame rate up to 18-20 fps (i.e. frame periodicity of 55.556 to 50 ms).
Using the mmwave demo visualizer also, I could use the record data button to capture some data. My questions as follows:
1. Is it OK to increase the baudrate?
2. Is there any other way to get 2D-FFT data from the sensor, preferably over UART?
3. How can I have access to 1D-FFT data?
4. Is there any scripts (MATLAB/Python) that can be used to load/read the captured .dat data from demo visualizer?
regards,
Tosin