This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: IWR6843AOPEVM versus IWR1443BOOST versus IWR1843BOOST

Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: IWR1843BOOST, IWR1443BOOST, , MMWAVEICBOOST, IWR6843AOP, IWR1843, IWR6843, IWR1443

Hi,

I was wondering what the basic differences are with the above listed devices- IWR6843AOPEVM, IWR1443BOOST, IWR1843BOOST...

From documentations I understand that I have to use the MMWAVEICBOOST board with the IWR6843AOPEVM for connectivity to the DCA1000 board. But this does not seem to be the case when I am to use the IWR1443BOOST or IWR1843BOOST. Could I know why this is so?

Will it be possible to have (in a custom design?) a direct connection between the IWR6843AOPEVM to the DCA1000 without using the MMWAVEICBOOST board?

-Tosin