Hi Alex,
After we have a meeting with customer yesterday, Customer now has two questions and I am also not clear, hope you can give some answer:
- the first is whether the data from the crosstalk calibration and the temperature phase calibration needs to be imported before the ambient phase calibration, and will the first two steps have an impact on the ambient phase calibration?
- The second problem is that our emitter led model is SFH 4556 with a measurement distance of 1.6m, the customer wants to reach 2m, and need the total angle of the 3 emitters is >90, Whether we need to re-select the emitter led , and if so, which led should we choose?
Could you please take your time to give me some answer or suggestions?
Thanks.