This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AWR1843AOP: AWR1843AOP mmWave SDK 3.5.0.4 demo elevation bug fix

Guru*** 148954 points
Part Number: AWR1843AOP

It was identified that the mmWave SDK 3.5.0.4 demo for AWR1843AOP provides incorrect elevation z value. The value computed by the demo has incorrect sign. For example, when correct elevation is z = 1m, the demo reports z=-1m.

This issue is due to incorrect Tx antennae numbering used in the demo.

In order to correct this issue please modify the following file as follows and rebuild the demo binaries as described in the SDK User Guide.

C:\ti\mmwave_sdk_03_05_00_04\packages\ti\board\antenna_geometry.c

Replace

ANTDEF_AntGeometry gAntDef_AWR1843AOP = {
     .txAnt = {
                {0, 2},
                {0, 1},
                {0, 0}
       },
     .rxAnt = {
                {3, 0},
                {2, 0},
                {1, 0},
                {0, 0}
              }
};

With

ANTDEF_AntGeometry gAntDef_AWR1843AOP = {
     .txAnt = {
                {0, 0},
                {0, 1},
                {0, 2}
       },
     .rxAnt = {
                {3, 0},
                {2, 0},
                {1, 0},
                {0, 0}
              }
};