Hi.
I am using awr1843aop with lab0014_obstacle_detection_aop in automotive toolbox.
When i enter sensorstart command, it works for a while. Then it stop working.
Then appear "MSS Exception: ../mss_main.c, line 2049." in my terminal.
I followed mss_main.c, line 2049. That was a kind of error message defined in sdk.
I don't know the reason why this error happen. But i guess that Number of detected points exceed the limitation.
I used GUI called ods_3d_visualizer TI served. And figure out what timing sensor stop.
I defined "ODSDEMO_MAX_OBJECTS = 65" (default = 50). However, it stops when the number of objects exceeds 65.
I don't understand why the output number of objects is exceeded 65.
TI blocked this situation by coding like this.
"if (cfarOut->numObjDetected > ODSDEMO_MAX_OBJECTS)
return CFAR_ERROR_MAX_DETECTION_EXCEEDED;"
Please let me know why this situation happening.