This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP112: Linux reads TMP112 tutorial in I2C form

Part Number: TMP112
Other Parts Discussed in Thread: LM75SW-LINUX

Hi team,

I help the customer ask a question.

"In order to read TMP112 data in Linux, I have configured the LM75sw-Linux driver in Linux kernel according to the official website TMP112 page:
Device Drivers --->
<*> Hardware Monitoring support --->
<*> National Semiconductor LM75 and compatibles

Add the following content to the device tree:
&i2c1 {
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c1>;
status = "okay";

tmp112@48{
compatible = "ti,tmp112";
reg = <0x48>;
status = "okay";
};
};
TMP112 ADD0 was grounded. According to the data table, its device address should be 0x48, which is consistent with the device tree.
After setting up the experimental environment, I want to read the contents temperature data of /sys/bus/ i2C /devices/0-0048/ temp1_INPUT .
Quention:
There is no temp1_input in /sys/bus/i2c/devices/0-0048/. Is the path of the data interface wrong?
If there are other configurations required to find the TMP112 data interface on Linux?"

Thank you very much for your help.

Best regards,