Can we use automotive demo lab0004_obstacle_detection in AWR1843Boost?
If not, what is the reason this demo doesn't work with AWR1843Boost?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can we use automotive demo lab0004_obstacle_detection in AWR1843Boost?
If not, what is the reason this demo doesn't work with AWR1843Boost?
Thanks
Hi Lei,
While you may be able to run the binary on the device, the lab will not output the correct results. This is because the ODS EVM has a different antenna pattern than the Boost EVM, and hence the signal processing chain will not be able to produce correct angle information when running on a different EVM with an antenna pattern it wasn't designed for. The distance and velocity information should still be reasonable.
Regards,
Aayush