Other Parts Discussed in Thread: TMAG5170UEVM, TMAG5170
Hello,
We are evaluating the TMAG5170-Q1 hall sensor and need to understand the behavior of the CONV_STATUS register update.
1. When we read the CONV_STATUS register without providing a trigger for conversion, the X, Y, Z and T status show value 1.
Is this an expected behavior, as 1 indicates the current value, but the conversion is never triggered ?
2. On triggering the conversion, and reading the CONV_STATUS immediately (SPI is in blocking mode), the status return 0, (Indicating the conversion is not yet complete and data is not available).
However reading the same after 10ms gives the result as 1.
3. Also Temperature result registers provides the temperature result without triggering the conversion, is this not dependent on the command for conversion ?
Could you please provide some insights on these observations
Thank you,
Aditya