Hello Everyone
The new mmWave Industrial Toolbox Version 4.10.1 is now live on TIREX. This package includes both new content and updates to existing material. The full release notes can be found below.
Industrial Toolbox 4.10.1
-------------------------------------------------------------------------------------------------------
New and Updated Features
Antennas
- IWR6843LEVM NEW
Labs
The following Labs have been updated in this toolbox:
- Out of Box Demo
- Added support for IWR6843LEVM
- People Counting Labs
- Added IWR6843LEVM to lab/evm support matrix
- People Counting with Vital Signs
- Now supports the AoPEVM in standalone mode
Bug Fixes
- Fixed broken links
- Fixed issue in People Counting Visualizer where default values would no longer fill in correctly due to Toolbox version number having an extra digits
- Fixed the cfg provided for Fall Detection
Packaging Updates
- Dramatically reduced package size through video compression and removal of unused resources
-------------------------------------------------------------------------------------------------------
Industrial Toolbox 4.10.0
-------------------------------------------------------------------------------------------------------
New and Updated Features
Labs
The following Labs have been updated in this toolbox:
-
- New lab category that contains labs that have basic modifications to existing content
- Labs in Fundamentals are made to serve as reference as to how specific features can be added to a mmWave Application
-
People Counting with Vital Signs
- New lab which demonstrates the use of TI mmWave sensors for Vital Signs Detection on a target from a wall mount position
- Leverages the tracker to localize the target location
-
- Allows you to combine People Counting using mmWave with SimpleLink WiFi in order to transmit radar data over the air
- Comes with premade binaries to simplify the flashing process
-
- Updated to use the newer methodology for Hard Coding a Configuration
Packaging Updates
- Reorganized directory structure to ensure consistency of content organization
- Added additional landing pages
Bug Fixes
- Fixed issue where tracker-based labs would not run after being recompiled.