Hi,
Recently I'm doing the research about human detection/fallen detection project in near range (around nearer than 5 ~ 10 meters). And I found that maybe the IWR6843 series (ISK, ODS, AOP) are suitable for me.
But many people mentioned that the demo programs run on these platform are not support or the related toolbox can not be download anymore, could you please give me the suggestion which programs now are currently available and where are those links can be accessed.
Further, I would like to know is there any possibility to capture RAW data while running these program? Maybe directly using the demo GUI or such as DCA1000 board? This is a quite important feature for my research.
And if the data are capturable, what kinds of the data I can get? The ADC-RAW data, or the point cloud data denotes in coordinates?
I'm looking forward for your advice and suggestions.
Many thanks,
Shihyu.