Hello expert,
I had 2 questions from my customer.
1) In the IWR6843Aop data sheet, it shows the EIRP result is 15dbm. What is this measurement under what conditions?
(For example, is the measurement resolution of the Spectrum analyzer setting 1MHz? Is the measuring position 1 m?) .
They would like to confrim this result in ther lab.
2) Have you also been tested for compliance with radio laws in Japan as a module?
If so, I would like to get a test report.
Regards,
A.Fujinaka