Hi Team,
Our customer would like to know if they can use the HDC302x-Q1 sensors to test the humidity in hydrogen gas. I have asked some questions from our customer and here are his response.
1. What is the operating pressure?
Ans.3 Bars
2. Can you please confirm the concentration range of hydrogen?
Ans. Could be up to 100% hydrogen
3. Is the environment completely free of oxygen and only hydrogen is present?
Ans. the sensor has to be used one time in normal air (with oxygen) and one time in a full hydrogen concentration
4. Could you provide the end application to help us determine the sensors behavior during hydrogen exposure?
Ans. It is used in a Hydrogen supply line of a fuel cell, as well as supply line of the air.
Regards,
Danilo