Other Parts Discussed in Thread: TDC1000
HI TEAMS:
TDC7200 enable has also tried to use IO control to pull up the enable after 3.3V power supply.
The current process is:
Chip power on - initialize SPI - enable pull up - write register
At present, register reading and writing are as follows:
After 0x03 is written in 0x00 register of 7200, it is not reset to 0 as specified in the specification
The schematic diagram is as follows: tdc7200
TDC1000