Other Parts Discussed in Thread: OPT3101, OPT3101EVM
Hi experts,
Now I'm trying OPT3101 estimator but I can't get the same results as one in the datasheet, page106.
Distance noise is about 2 times worse than the value in the datasheet.
(my result is 210.06mm at 5m of target distance)
My setting is bellow.
Average Sub-Frame Count : 128
Number of sub frames : 128
Samples per second : 31.25
Expected Ambient Current Value : 100.0
Ambient Lux : 130.00
Mode of Operation : HDR
HDR Ratio : 64
Distance Between LED and PD : 5.00mm
LED Model : SFH4550
PD Model : SFH213FA
Target Distance : 5000.00mm
Reflectivity : 18.00%
Are there anything wrong? or Could you give me some advice to get the same results as the datasheet.
Now I'm not confident any of my results simulated by OPT3101 estimator.
Best regards,
Tsutomu Hattori