This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP275: Interfacing with 1.5V LVCMOS IO

Part Number: TMP275
Other Parts Discussed in Thread: TMP114

I am planning on using the TMP275 for on board temp sensing. It runs off 3.3V, but looking at the digital logic threshold, it's not possible to interface with 1.5V LVCMOS logic. Is there a solution for interfacing with 1.5V IO or is a temp sensor that will be able to run off of 1.5V with an I2C interface with similar performance as the TMP275?