Hi,
I would like to ask please 2 questions:
1. What parameters define the repeatability of the sensor ?
2. How does the calibration process should be done?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to ask please 2 questions:
1. What parameters define the repeatability of the sensor ?
2. How does the calibration process should be done?
Thanks
Hi Yoav,
Thank you for posting to the Sensing forum.
The TMP144 does not have repeatability specified in the datasheet. I will look to see if there is more information we can provide and update this thread.
The host will send a calibration byte to allow the TMP144 to sync to the baud rate of the host. This protocol is described in more detail in section 7.5.1 of the datasheet, and the calibration byte is shown in figure 7-4:

Best regards,
Nicole
Hi,
Anything new about the repeatability ?
About the calibration, I meant that if I need to write to the sensor offset temp, or something like that ?
Thanks
Hi Yoav,
There's no need to calibrate temperature accuracy. TMP144 meets the temperature accuracy as outlined in the EC table. Repeatability is expected to be within Typ spec.

thanks,
ren