Other Parts Discussed in Thread: IWR1642, UNIFLASH
Hi everyone,
I'm trying to reuse the existing project in labs under industrial toolbox (4.11), i followed step by step indications on how to use the 3D people counting on my board (IWR1642) but i'm still having some questions, here it is :
- One of necessary procedures is to flash the 3D people counting project is to flash the 3D counting image (bin file using uniflash) on the EVM, is there a way to know what is the current image flashed on the board? and,
- will the image on EVM will be reset after NRST button pressed or card restart (deplug and replug the power supply)
- Is the image (bin file)/the lab compatible with the IWR1642 card especially it was not mentioned here that the lab is compatible with it (hardware requirements :IWR6843ISK or IWR6843ISK-ODS or IWR6843AOP or IWR6843L)
- When starting the in the GUI mode, should i pass the PINs (SOP0 SOP1 SOP2) on card to functional mode or i have to let it on flash mode (001 or 101) : i'm know passing to the functional mode.
Responding to these questions will help me so much, so thanks in advance.
Best wishes.
Abdellah.