Other Parts Discussed in Thread: IWR1642, IWR6843
Hello TI community,
I'm trying to follow this guide for short range radar detection, i succeed in all the steps until 6th (the GUI is launched and plotted). in the other hand i tried to follow developer's guide as well, i installed the software requirements and also verified the installations (everything's good), i imported both projects on CCS (DSS and MSS as mentioned in the guide) and tried first to rebuild the dss project. A successful build generate a .bin AND a .xe674 files but in my case only the .bin file is generated !!
Knowing that i'm having this two strange error/warning on the CCS console :
- The error : process_begin: CreateProcess(NULL, rm -f C:/Users/<my name>/workspace_v11/srrdemo_16xx_dss/srrdemo_16xx_dss.bin, ...) failed.
make (e=2): Le fichier spécifié est introuvable. (means the file is not found)
gmake[1]: [pre-build] Error 2 (ignored) - The warning : warning #10370-D: Possible codesize or performance degradation. Section ".text:SOC_init:libsoc_xwr16xx.ae674<soc.oe674>" has calls to rts routines, but rts is placed out of range from call site at 0x20003604, or in a different section. To optimize codesize, either 1) place rts closer to call site, or 2) place rts in same section, or 3) compile with --disable_push_pop.
warning #10370-D: Possible codesize or performance degradation. Section ".text:SOC_init:libsoc_xwr16xx.ae674<soc.oe674>" has calls to rts routines, but rts is placed out of range from call site at 0x200034e0, or in a different section. To optimize codesize, either 1) place rts closer to call site, or 2) place rts in same section, or 3) compile with --disable_push_pop.
So my questions are :
- Is the build successful ?
- How to verify that the mmwave device support packages are up to date (later than 6.0.0576) as indicated in the guide ( in Software Requirements)
- About another project building : I've noticed on the lab directory that there is no compatibility between the EVM i'm using (IWR1642) and a project i want to build (3D people count) is there any way to make it compatible or emulate the needed device on my device? if not what's the reason that make a project compiled on a kind of EVM and not another kind (hardware or software)?
Thank you in advance for helping.
Best regards.
Abdellah.