Hi Expert,
My customer is using DRV5056-Q1 is their new project. Have some questions for the calculation tools on ti.com.
There are 3 different calculation tools for DRV5056-Q1. Customer would like to use it to calculate the magnetic for linear movement. So which tool should they use?
Besides, they tried with tool 1, when the distance between magnet N45 Φ5*8mm and the surface of DRV5056-Q1 is 2.8mm, the calculated magnetic flux density is 156mT.
If they use tool 3, when the distance between magnet N45 Φ5*8mm and the surface of DRV5056-Q1 is 2.8mm, the calculated magnetic flux density is 120mT.
So which tool should Customer refer to?
Thanks!
Ethan Wen