Hi ,
We are using AWR2243 board and connecting it to an external host. The DFP porting to the external host is done by following the TI dfp porting guidelines. The meta image v2.2.0.3 is used, which is of size 334656 bytes.
The firmware download is taking more time than expected in external host. To cross verify the timing this we checked the same AWR2243 board with the TDA2x board. We observed TDA board and the firmware download is happening significantly at a faster rate.
The timing for the firmware download with two boards are as follows,
With TDA board: 2.95s
With external host: 3 minutes and 20 secs.
We would like to know the reason why it is faster in TDA board and implement the same in external host. Please let us know how to resolve this issue.
Thanks and regards,
Srinivasan