Other Parts Discussed in Thread: TMAG5170
Dear Sir, Madam
I saw on the datasheet of the component the current consumption in continuous conversion mode is about 3.4mA, however it is written in "test condition" it was done with /CS high. So I would like to know if this consumption is when we put a "high" level in input of the pin (so the system doesn't communicate in SPI) or when the pin is in "high" level (so we put a "low" level in input of the pin and the system communicate). If it is the consumption when the system doesn't communicate, could you give me the current consumption when the system is in communication in continuous conversion mode please ?
Is the CORDIC algorithm editable by the user or not ?
Is the use of CORDIC modify the current consumption ? If it is, what is the current consumption ?
I look forward to hearing from you.
Arnaud LANDRI