Dear TI Team,
I am trying to use CANFD communication in the demo example lab0014_obstacle_detection_aop by using the reference from lab0005_object_data_over_can.
and also referred the following documents and threads
1)https://www.ti.com/lit/an/spracf7/spracf7.pdf
2)https://www.ti.com/lit/an/swra606/swra606.pdf
But when I build the project in CCS I am getting the following error
subdir_rules.mk:9: recipe for target 'mss_main.obj' failed
"../mss_main.c", line 2312: warning #169-D: argument of type "CANFD_MCANInitParams *" is incompatible with parameter of type "uint8_t"
"../mss_main.c", line 2312: warning #169-D: argument of type "int32_t *" is incompatible with parameter of type "const CANFD_MCANInitParams *"
"../mss_main.c", line 2312: error #167: too few arguments in function call
1 error detected in the compilation of "../mss_main.c".
gmake[1]: *** [mss_main.obj] Error 1
makefile:153: recipe for target 'all' failed
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
How to solve it?