Hello,
from the datasheet, DRV5056 has a quiescent voltage of 0.6V ; and the output voltage will be below this value if the device is subjected to a 'negative' magnetic flux.
I plan to use a couple of DRV5056 with a MCU.
My early experiments shown that when subjecting a DRV5056 to a negative magnetic flux, the output voltage goes down to a value of "26" (after conversion by ADC, i.e. 0.12V approx)
My questions are:
1) is it the reliable to rely on this property to discriminate 2 magnets ? or does this "property" is subjected to changes/variations between products (even products of a same batch) ?
2) is it safe to submit "permanently" a DRV5056 to a negative magnetic flux ?
Thanks