This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: i am looking for any data sets for iwr6843 or awr6843 using the three tansmitters

Part Number: IWR6843

hello, 

currently, I am working on a signal processing chain on matlab that takes the ADC data and produce the point clouds but in order to test this signal processing chain I need some data sets to experiment with it 

but I don't have the hardware so I was wondering if there are any data sets of ADC data with these sensors with known configurations that uses the 3 transmitters I am asking for the 3 transmitters because the processing chain 

also, estimate the elevation angle and it would be better if the data set was captured with 3 transmitters to get better resolution for elevation angle and also it would be good if these data sets are recording known targets so that I can expect the results.

thanks alot