Other Parts Discussed in Thread: IWR1843BOOST
Where are the various temperature sensors located on the IWR6843AOP?
The mmWave Demo Visualizer displays the device temperature report from various temperature sensors in "Profiling".
(The capture below is shown using IWR1843BOOST.)
The "rl_sensor.h" in mmWave SDK defines various temperature sensors, which seem to correspond to the temperature sensors in the device temperature report in the mmWave Demo Visualizer.
C:\ti\mmwave_sdk_03_06_00_00-LTS\packages\ti\control\mmwavelink\include\rl_sensor.h
The following posts about the location of the temperature sensors.
e2e.ti.com/.../4101940
e2e.ti.com/.../3751790
Is each RX temperature sensor located next to the LNA?
Is each TX temperature sensor located next to the PA?
Is the PM temperature sensor located next to the internal power circuit?
Is each digital temperature sensor located next to R4F or C674x?
Best regards,
Daisuke