Hi,
We are communicating to AWR2243 sensor using a host processor. We have successfully ported the mmWave DFP to the host processor.
While receiving raw data over CSI2 data, we occasionally get a DFP message saying Async even handled invoked f:80. Based on our search, this error means that the capturing data time is more than the frame time.
If this is the case, since we are using AWR2243, the frame period is fixed and should not vary from frame to frame to cause this error. Additionally, when using infinite frames, this doesn't seem to happen. After this message from Async handler, the CSI2 data stops streaming.
Our active frame time is a little less than 10ms while our frame time is 50ms.
Can you help us identify why this error pops up from DFP occasionally and how to handle it?
Thanks in Advance,
Santhana Raj