Hi all,
I hope you are doing well. I have several questions regarding the usage of the TMP461 that I am looking for answers on:
Q1) Does the TMP461 treat the voltage developed between the D+ and the D- pins as a true differential signal implying the D- input is high impedance? If D- input is low impedance, what is its impedance with respect to GND (pin 6). If D- is high impedance what is the maximum & minimum common mode voltage allowed on D+ and D- ?
Q2) What is voltage to counts transfer function that maps the (assumed differential voltage between) D+ and D- that corresponds to 0 through full scale A/D counts.
Q3) What is minimum bandwidth needed for the A/D to read accurately at each of the 3 measurement currents?
Thank you for your support on this and I hope to hear back from you soon.